I want to create a simulation in TINA with LM10, LT1101, LM1558 in the design (existing design in a current product). However, none of these are in TINA or SPICE for simulation. Can anyone suggest equivalent models?
If LT1101 is an IN Amp, so if nobody can suggest a similar model, I am going to use INA827 (will set a gain of 10 with 16k resistor, as the LT1101 is configured as gain=10). LM1558 looks to be just a run-of-the-mill OpAmp, so I will use LM 258.
LM10 is a little more tricky... it has the built-in reference op amp (which is the portion that my current product design uses. Ideas??