This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can you provide the required Clearance and Creepage Distance for the ISO121BG ?
Is this information available?
Thank you!
Hi Jim!
I hope you're doing well.
I went to the TI packages site: http://www.ti.com/packaging/docs/searchtipackages.tsp?packageName=DIP
Identified the package type as CDIP SB JVD from the datasheet.
Found the associated package drawing from the packages site: http://www.ti.com/lit/ml/mcdi039/mcdi039.pdf
Creepage is the shortest distance between two conductive parts measured along the surface of a solid insulation.
Clearance is the shortest distance between two conductive parts measured through air.
I'll use nominal values in inches for the calculations.
Creepage: 2*((0.065+0.030)/2) + ((0.610+0.580)/2) = 0.69 inches
Clearance: ((0.012+0.008)/2)+ 0.6 = 0.61 inches
Provided a picture to help the customer understand where my measurements came from.