Part Number: INA210-Q1
Hi team
INA210-Q1 D/S say Input bias current = Max 35uA .
[1] so total input bias current would be Max 70uA(= 35uA x 2) for two input pins ?
[2] further, may I know total input bias current for two input pins at Vs = 0V and common mode voltage = 20V ?
[3] figure 11 and figure 12 are showing Ib for only each pin, so that I have to double the graphed Ib for two input pins ?