Part Number: LMC6484
Other Parts Discussed in Thread: LM35, ADS1100, LMC6061, OPA317, OPA388, TLV333, OPA376
Hello,
I'm using LMC6484 to convert a LM35 temperature signal (about 0 - 70° C) into a 0-5 V range which is then fed into an ADS1100.
I chose the LMC6484 as it was used in a similar existing design ;-) Now I'm looking for a replacement as I'm only using a single op amp of the LMC6484. It is operated as a single-supply (5V) non-inverting operational amplifier. See attached circuit.
What would be a good replacement, e.g. would a LMC6061 or OPA317 work as a "drop in" replacement? In terms of voltage offset and drift they match or surpass the LMC6484 and I think their lower GBW is of no relevance.
Thanks!