This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm using LMC6484 to convert a LM35 temperature signal (about 0 - 70° C) into a 0-5 V range which is then fed into an ADS1100.
I chose the LMC6484 as it was used in a similar existing design ;-) Now I'm looking for a replacement as I'm only using a single op amp of the LMC6484. It is operated as a single-supply (5V) non-inverting operational amplifier. See attached circuit.
What would be a good replacement, e.g. would a LMC6061 or OPA317 work as a "drop in" replacement? In terms of voltage offset and drift they match or surpass the LMC6484 and I think their lower GBW is of no relevance.
Thanks!