This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using INA181 current sensor. I am facing the problem that it is not giving the desired output. On varing the Input Supply the output is not changing. On giving a few mA current, the output gets saturated to a value. I don't if my circuit connections are wrong or what's the problem. Someone please resolve my issue.
Hi Sushant,
you have drawn a chip with 5 pins. That's not the INA181. Do you mean the INA180?
Also, you don't have connected a Rsense across the inputs. And where is the lower end of 330R resistor connected to?
Please have a look into the datasheet to see how the chip has to be wired.
Kai
Hi Sushant,
take care, the INA180/181 only withstands an input voltage of 26V. So, a 30V supply as shown in your schematic will be too much.
The following simulation shows what happens when you connect a Rsense of 1R between the input terminals:
Whether a Rsense of 1R is a proper value depends on your application and whether the voltage drop across Rsense is tolerable. You can decrease the voltage drop by decreasing Rsense. But then your output voltage also decreases. Also, when decreasing the voltage drop across Rsense the input offset voltage becomes more and more dominant. The input offset voltage of INA180/181 is 500µV maximum and creates an error of up to 1% if the voltage drop across Rsense is 50mV.
Here's the TINA-TI file:
Kai
Hello Sushant,
Thanks for considering to use Texas Instruments. How is your input current varying? The above diagram corresponds to a single operating condition. If V2 varied from 4V to 6V or something else, I would expect that you would see the output change. How I see it there are two ways to observe the device operation. One is to vary V2, the other is to replace the 330 ohm with an electronic load or potentiometer. Both of these are illustrated below.