This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
This is Gordon Liu of WNC in Taiwan.
I want to use OPA2674 be a RF PA(13MHz).
Its OP1dB is only 19dBm on the below circuit that don't meet datasheet 350mA@12V.
Could you teach me where wrong is??
12V DC_In (mA) | Pin (dBm) | Pout (dBm) | Gain (dB) |
30 | 0 | 12 | 12 |
32 | 1 | 13 | 12 |
32 | 2 | 14 | 12 |
34 | 3 | 15 | 12 |
36 | 4 | 16 | 12 |
40 | 5 | 17 | 12 |
42 | 6 | 18 | 12 |
44 | 7 | 18.6 | 11.6 |
46 | 8 | 18.9 | 10.9 |
48 | 9 | 19.1 | 10.1 |
50 | 10 | 19.2 | 9.2 |