Other Parts Discussed in Thread: OPA132,
Can you explain to me why with this type of schema, programmable via the ADG441 a gain of 1 or a gain of -1. We need to change the OPA2132U IC92 after a
few months of use due to off-specification output offset> 0.5μV
Ex de mesure:
|
Carte H447 |
Point mesure |
||||||||
|
Consigne |
IC96-1 |
C404 |
IC92-7 |
||||||
|
1V |
0.19937 |
0 |
-0.19721 |
||||||
|
-1V |
0.19936 |
0.19936 |
0.20145 |
||||||
|
|
|
|
|
|
|
|
|||
On the IC92-7 pin we have a difference of 0.20145-0.19721 = 4.24mV totally abnormal compared to the amp specification which gives a max offset of ± 0.5mV