This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
My customer is using LMH6518 in the 500MHz bandwiidth DSO application. A large offset (hundreds of mV) is observed when the output of LMH6518 is over drived under 500MHz. Is this normal? What can we do to solve this problem?
Thanks
Hello Kai,
The input and output are DC coupled, single ended input differential output. VIN+ is used as a signal input, and VIN- is a fixed 2.5VDC. VCM=1.25V. Put a 2.5V Offset, 560mVpp, 500MHz signal into VIN+ and measure the output of LMH6518.When 6518 is configured as 0x40a (LG -1.14dB), 6518 output is normal.
But when I configure HG =34.86dB, there is a large offet, and the ADC can not sample any AC signal.
Figure 1 0x417(HG 24.86dB)
Figure 2 0x413(HG 34.86dB)