This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can you suggest any peak detector circuit which can detect input voltage range of 0-3.3v peak @100k hz and using supply voltage of 3.3 v.
I tried some of the peak detector circuits using TI components..but there arent accurate..there is a difference of 20 mv between the input and output.
It would be highly appreciable if you suggest a peak detector circuit with the error difference < 3mv...Please also send the splice models files for the corresponding circuit so that i can verify ..
Hi Nandini,
it's hard to rectifiy a 3.3V input signal when the supply voltage of OPAmp is 3.3V.
Can you show us some of the circuits you experimented with?
Kai