Hi team,
My customer want to use the DRV595 to drive TEC in Atlas system. Please help to answer below question:
1. They has two 5W TEC in the system, the supply voltage is 12V. Can the DRV595 drive two TEC?
2. For the LC filter design in the datasheet
1) What's the ESR requirement of the C1 and C2? Can we use the ceramic capacitor?
2) What's the requirement of the Inductor? Such as the DCR. How to choose the Inductor. Does the switch frequency and the power of TEC decide the chosen of the TEC?
Lacey
Thanks a lot!