This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB2ANY: Address not acknowledged (NAK). Error -44

Part Number: USB2ANY
Other Parts Discussed in Thread: TPS65400

I have a problem using USB2ANY, I can open communication, set SMBUSControl and do other stuff but when I try to write bytes using 

u2aSMBUS_WriteByte

I receive error -44 that, according to your documentation, means "Address not acknowledged".
We are using firmware version 2.8.2.0 and DLL with same version.
The slave address I'm using is 0x6A (Evaluation board) which is the number I can read through PICommander (if I install an earlier version compatible with that software).

Regards

Enrico Bonacini