Part Number: INA114
Other Parts Discussed in Thread: INA202, INA190
Hi
I re-open this subject
The generator now delivers stable 29.56 ua
but il need to add a current monitor which will control max current about 1MA in case of problem with tue generator
I've chosen an TI INA202
I insert a shunt of 10 ohms between generator and load which car vary between 100k and 350 k as already explained before
I get the following problem
load under 200 k .. the current generator pass from 29.56 to 30.5 uA ?????
not a big problem but
when I put a
300 k load .. current fall to 25 uA !!!
I don't understand why ? I've checked that 2.5 V is always on resistor 91k of the generator..
I know that a part of current is to the inputs of the INA 202 but?
Could you help ?
if necessary I will post a new subject..
Thanks