Part Number: LM2901
In the LM2901 datasheet, table 7.8, it states that the Iol at a Vol of 1.5V is a minimum of 6mA. Does that mean that the output can only be guaranteed to sink 6mA? Or is it saying that at Vol = 1.5V, the amount of current it can sink is at least 6 mA, but typically 16 mA.