Part Number: AMC1200
Other Parts Discussed in Thread: AMC1100
I have trouble with following two circuit diagrams. they are from two reference designs for voltage measurement using amc1200. Two circuit diagrams are same except at the points which i circled. In one design, diode and one input terminal is connected to the ground. it uses 0-5V power supply to power the HV side . In the other design, diode is connected to the negative 5v and one input terminal is connected to the ground. It uses -5V-0- +5V supply. My question is, what is the difference between this two. Clearly one circuit design is wrong because all other factors are same except those points.
I obtained these circuits from tidua58 and tiduby7a.
Thank you.