This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Yes the simulation is correct, but can you to give me the equations for Zdiff = 800K and Zemc = 200K ?
Thank you for your help.
Yvan,
Attached please find the simulation file and free Tina-TI simulation tool used to simulate the common-mode and differential input resistance. VCVS with gain of G=-1 is used to drive the differential input of INA149 with two equal magnitude signals, which are 180 degrees out of phase, so the input common-mode voltage stays at zero.
e2e.ti.com/.../INA149-Rin_5F00_diff-and-Rin_2D00_cm.TSC