This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am designing a precision rectifier circuit for one of my design. Here the input is from current sense transformer and this using differential amplifier it will be converted to single ended.
I am using an precision rectifier to convert that AC to dc. Please find the attached circuit. The part used is LMV342IDGKR. I have see that " Input voltage (either input) –0.3 5.5 V " in the datasheet. Can you tell me the attached circuit will work without any issue.(Simulation is working fine)
If not can you suggest a part which suits for rectifier application with the package of "2 Circuit Rail-to-Rail 8-VSSOP"
Regards
Anuraj NK
Hi,
The part LMC6482 meets my design requirement. But the maximum operating temperature is 85Deg. I am looking for a part for -40 to 125 Deg. Can you suggest a part which meet this.
Regards
Anuraj NK
Hello Anuraj,
The LMC6492 is the extended temperature range (-40 t o125) of the LMC6482. Basically the same device, but the limits are slightly wider due to the wider temp range.