This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello everybody,
I'm using the LOG114 exactly as depicted in the Datasheet on page 11 in dual supply configuration, I1 derived from the internal 2,5V with 2,5MOhms. The design is powered by a single 3.3V voltage source. The +-5V are derived as described in Figure 12 on page 19 on the datasheet.
The current, that has to be measured, is created by a reference voltage of 1V followed by a variable resistor. If the resistance is low (~100k) i have no problem. However, the vlogout signal is very very noisy. This gets even worse if the current to be measured gets lower. It seems the chip starts to oscillate.
Do you have any idea, what to do about it?
Best Regards
Christof
Hi Christof,
how do you generate the 1V reference voltage? Is it clean, stable and noise free?
How far is the resistance away from the LOG114? Is there any cabling? Keep in mind that the LOG114 is a high speed logarithmic amplifier and doesn't like stray capacitance at the input pins 3 and 4.
Another issue is the +/-5V supply voltge generation. For a test you could power the LOG114 by linear voltage regulators providing +5V and -5V. Do you see an improvement then?
Scope plots would be helpful and a photo of your setup.
Kai
Hi Kai, Hi Tim,
thanks for your answers. It seems, that the mentioned stray capacity is indeed the problem, I was able to connect a 50Meg Ohm resistor directly between pin 3 and pin 16. Although the signal is still noisy, the ic itself doesn't start to oscillate and my ADC reads a voltage close enough to the resistors real value. However, without cables, the setup is of no use to me. Actually, not only cables are problematic in my design. The log114 is mounted on a separate board, which is connected to the actual sensing equipment through a pci-express edge mount connector, which introduces quite some capacitance! Is there any workaround to reduce the influence of the stray capacitance.
Could a current mirror, closly attached to the input pin of the log114 mediate this issue, or would this also cause capacitance issues? Do you have any recommendations?
Best regards
Christof
Hi Dennis,
sorry for the delayed response. I'm just now circling back to the project. The idea of using an external TIA for I->U to I conversion is quite interesting.
I'm trying to simulate this in TINA, however, I can't find a suitable OP-AMP for the first TIA (that converts the current to the voltage). I'am expection currents
as low as 1nA. Do you have a suggestion for me, which OP-AMP could be used to archive the proposed solution? I'm using the reference circuit from the
LOG114 page, removing the I2 source and replacing them with the TIA followed by a simple resistor.
Thanks for the help!
Christof
Hello Christof,
For very low input current transimpedance applications CMOS and JFET input op amps are the best choices to minimize input current related errors. Since you are interested in converting a current level as low as 1 nA to a voltage output, an op amp having a few pA of input current should work well.
The OPA376 is a high performance CMOS input op amp having a typical input bias current of 0.2 pA, and a maximum of 10 pA, at TA = 25°C. You can find the datasheet here:
http://www.ti.com/lit/ds/symlink/opa376.pdf
If you find there are other parameters that are important in your TIA application that the OPA376 doesn't quite meet, let us know and we can help recommend different amplifier.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hi Thomas,
thanks for the help. I followed your advice and implemented the OPA376 as TIA in my TINA simulation. The file i'am unsing is the SBOS301A from the website. When i do the dc transfer characteristics analysis, i vary the input resistor from 100Ohms to 1G, the result is however not satisfying. I'am trying to attach the file, what am i doing wrong?
Best regards
Christof
Hello Christoff,
I see in your TINA simulation that you have an input current to the LOG114 of 1 mA. Do note that the LOG114 log conformity begins to degrade with input current levels above 1 mA. This is evident in the graphs on Page 7 of the datasheet. If you can keep the maximum input current lower than 1 mA by increasing the resistance of the TIA series output resistor, better log conformity performance can be achieved.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hi Thomas,
thanks for the advice, actually i don't think my signal will exceed 1mA.
Best regards
Christof
Hi Christof,
Do you have all the information that you need for your TIA/LOG114 application? If so, could you please close this e2e thread? If you have questions later, you can always start a new e2e post.
Regards, Thomas
Precision Amplifiers Applications Engineering