This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BUF634: Using BUF634 as a mid-rail splitter with unbalanced load

Part Number: BUF634
Other Parts Discussed in Thread: TINA-TI, OPA2810,

Hello,

I am using BUF634 to derive a mid-rail virtual ground in a 24V single supply system, thus creating a +12V and -12V dual supply.

I have a constant load of 50mA that draws its current from the positive side of the virtual ground.

When simulating this in TINA-TI - I see a significant decrease (about 0.5V) in the mid-rail voltage. Instead of 12V I get 11.5V.

This can be solved by applying a constant load by a resistor between the -12V and the virtual ground, but I was hoping to avoid having to use such a resistor (0.6W).

To clarify - I use this virtual ground for other parts of the circuit - so need it to be stable and exactly in half point.

Is there another way?

thanks

Uri