This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Searching suitable quadruple op amp as buffer for ADC

Other Parts Discussed in Thread: LMV324, LM7705, LMV844

Hello,
I searching a suitable rail to rail quadruple op amp with minimum offset and a negative rail swing very close to GND. I want to use two of them as buffers for an ADC (MCP3204).
I have a 5V single supply voltage and tried to use the LMV324 - but the output swing of the negative rail is about 50mV without 0V signal input.
That is to much for my application because it's a zero based measurement. Is there an opamp with better data for my application or what can i do instead?

Note:
I need rail to rail because i want to drive with the other two op amps two logic level Mosfets. In fact this capability is working with the LMV324

Best Regards
Wolfgang