Part Number: ISO122
Other Parts Discussed in Thread: ISO224, AMC1311
Please, answer another question
If I will use ISO122, can I use circuit in attach? Please, see attach.
TIA
Sincerely,
Vladimir Naumenkov
www.agat.by
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Vladimir,
I cannot answer this question because the datasheet does not have enough data. Maybe a TI's employee will be able to answer this question.
When powering the chip with +/-15V, the input voltage range is +/-12.5V typically and +/-10V guaranteed. So, it seems that the input voltage should stay 2.5V (better 5V) away from the supply rails. This could mean that the ISO122 will provide an input voltage range of +/-2.5V typically, when powered with +/-5V. But it can also mean that due to manufacturing tolerances some ISO122 might not work at all even with a vanishing input signal.
Remember that the ISO122 is from 1989. At this time OPAmps and isolation amplifiers like the OPA122 were usually powered with a bipolar supply voltage of +/-15V. The modern TI's AMC series, on the other hand, is free from these restrictions and can be powered with a single supply voltage of +5V.
Kai