Part Number: TL084
Hi Team,
My air conditioner customer has some problems about the TL084 current acquisition circuit. (Circuit below and attached tina files)
The +/- 8V (maximum range) sin signal @60Hz comes from the Hall sensor, then it is inputted to the inverting port of the amp through the divider network (R1, R2,R3). The gain is set at G=2. normally the output should vary around 0 level, thus +/- 3.46V (maximum range) sin signal @60Hz.
Finally, the +/- output signal will be translated to 0 ~ 3.3V signal, which is compatible with the MCU sampling port.
Now customer has 2 problems:
1. zero-input drift. when there has no current on the line, hall sensor has zero voltage and output should have zero voltage, but the output signal of the amp has voltage amplitude higher than 0.26V (threshold set by the MCU), triggering FAULT message.
2. Low temperature and high humidity working environment (condensate water around TL084): it still has no current on the line, hall sensor has zero voltage and output should have zero voltage, but the output signal of the amp has voltage amplitude @ 3.1V, triggering FAULT message.
These 2 problems are not easy to re-occur and customer are going to MP at the beginning of next month, could you help analysis?
Thank in advance and best regards,
Yang WU
TL084 current acquisition circuit.TSCTL084 Stability analysis.TSC