Part Number: OPA548
OPA548: We have a situation where we are following a circuit very similar to your Evaluation board SBOU132 (Figure 1) including the "Motor " Diodes (D1/D2) where we have a solid DC voltage going into the inputs of U1. the output has a 1:1.5 transformer across R6/C8 which is probably sinking any output. The reason we have DC is our VDD and VSS PS are left on during test and put about approximately 6.5 VDC on U1-1 and U1-2. When this occurs we get about 70 DegF rise on the op-amp a jump up from 70 nominal. We are well within the thermal parameters of the op-amp is there any concern about long term stays in this condition?