We are concerned that our simulation does not represent or indicate a failure we are having sow we want to see the schematic of the die and maybe simulate that or at least use it to analyze the failure we are seeing.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are concerned that our simulation does not represent or indicate a failure we are having sow we want to see the schematic of the die and maybe simulate that or at least use it to analyze the failure we are seeing.
Hi Robert,
TI does not openly share die images, or detailed die schematics, due to the proprietary nature of many designs. Some general information such as a die image may be included in the datasheet if the product is offered as an unencapsulated die. Also, some datasheets do provide a simplified schematic for the product. That is not the case for the OPA548.
The best option as Kai mentioned is to provide us information about the OPA548 failure you have experienced. We will need to see your circuit schematic, power supply voltages, input signal details, and output load conditions on the op amp. More information may be needed if we can't make a determination from what is initially provided.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hello Robert,
The OPA548 is a very popular TI power op amp that provides reliable operation when properly applied and protected. Can you tell me anything about the output load after the 1:1.5 transformer? Back EMF can be an issue with reactive loads and when that is the case external protection of the op amp is necessary. Datasheet Figure 38, Motor Drive Circuit, shows how current steering diodes are used to protect the OPA548 from back EMF generated by the motor. Today, we would add TVS diodes to the power supply pins to provide a current path for current associated with the EMF event.
Any information you can provide would be helpful.
Regards, Thomas
Precision Amplifiers Applications Engineering
Output load of failure is a .01 uf and 45 ohm resistive load in parallel in a test environment and we have the diodes in like the motor drive circuit
Hello Robert,
Our applications support of the Precision Amplifiers e2e forum is mostly of a technical nature and we don't have involvement in establishing an NDA between TI and our customers. I suggest that you contact the TI field office in your region, or the authorized TI distributor from who you purchased the OPA548 devices and ask them about what is required to have an NDA put in place between your company and TI. They should also be able to check if an NDA is already in place between the two companies. If so, that makes exchanging confidential information much easier and faster.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hi Robert,
is the OPA548 an original TI's component? Or could it be a conterfeit? Have you bought the OPA548 from an authorized TI's distributor?
Connecting a transformer to the output of an OPAmp can be tricky. A transformer can present a short circuit at DC. Have you AC coupled the transformer to the output of OPA548? Also, have you mounted the Zobel network as recommended in figure 38 of datasheet?
Are you sure that the OPA548 is not oscillating? Does it become hot?
Inductive kick backs can easily destroy the output of an OPAmp, if not protected. Have you mounted the free wheeling diodes very close to the OPA548 pins? And don't foget the TVS across the supply terminals of OPA548 as suggested by Thomas!
Can you insert an isolation resistor at the output? This could decouple a bit the complex load from the feedback loop of OPA548. And it could be used to provide a robust two stage free wheeling protection.
Kai
We have the motor diode in but how are the TVS diodes your talking about placed in the circuit, is there a diagram?