This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Would anyone know if the Burr Brown REF200 100 uA Current Source IC and .01 uF capacitor would be needed for conditioning the 50 ohm output of a Keysight 32210 Function Generator.
Planning to use it to amplify the current using an output of 10 hertz, 5V0-pk square wave.
Application is being used to drive a pair of Helmholtz coils which require a unipolar 1 Apk square wave of current.
Resurrecting an old design and am unsure if this signal conditioning is needed as a 555 timer was used previously.
Hi Tim,
can't see the schematic... :-)
Can you post it again? Click the "Insert Code, Attach Files and more..." button. Then click the "Insert File" button in the header.
Kai
Thank you Kai.
The previous has been added to the attached word file and depicts it use with a 555 timer, LCC110 photo diode, and +5V, and -5 V rails.
The Helmholtz coils will be the same and have a input resistance of 5.6 ohms and inductance of 6 uH.
The resistor shown in the output is not shown correctly but is intended to be the current limit resistor RCL presented in the datasheet.
Its value of 0.4 ohms is based on equation 1 of the datasheet using a 2 A limit.
Figure 13 recommends fast recovery diodes but does not recommend a part number.
Kindly recommend a fast recovery diode.
Also please confirm the filter capacitors chosen.
Their values are based on 50 KHz and 50 MHz conducted susceptibility requirements and the "Rule of One" commonly used for AF and RF electromagnetic compatibility.
Also need a recommendation on heat sink.
The note recommends a Waekfield-Vette 345 series I trust will be meet the needs we have at zero g and 30 C max ambient air and 1 A max and 5 V or 5 W max continuous current draw.
Finally please confirm that the TO-3 package chosen is not recommended and confirm that a TO-220 package would is recommended.
I have also added 100 KOHM and 50 KOHM feedback 1/4 W Input resistors and IN4003 diodes.
Hi Tim,
Figure 13 recommends fast recovery diodes but does not recommend a part number. Kindly recommend a fast recovery diode.
ES3BB-13-F
Additionally, it is recommended that transient voltage suppressor diodes be added from each supply pin to ground as shown here:
The TVS reverse standoff voltage (VR) needs to be somewhat higher than the supply voltage levels you intend to use. You can get more information about TVS diodes at this website:
https://www.littelfuse.com/products/tvs-diodes/surface-mount/1ksmb.aspx
Also please confirm the filter capacitors chosen.
I presume you are speaking about the OPA541 power supply bypass capacitors? If so, 100 nF ceramic capacitors connected directly from the OPA541 +V and -V pins to ground. Larger capacitance 10 uF capacitors are recommended on those power supply lines as well, but they can be located more distant from the +V and -V pins.
Also need a recommendation on heat sink.
The datasheet recommends the Waekfield-Vette 345 series heat sink as you noted. That heat sink is recommended for high power applications where the OPA541 must dissipate many watts of power. A complete thermal analysis associated with the OPA541 operating conditions would be needed to see if something less substantial could be used for the heat sink.
Finally please confirm that the TO-3 package chosen is not recommended and confirm that a TO-220 package would is recommended.
The OPA541 in the TO-3 package is not recommended for new designs (NRND). That means that version of the OPA541 will cease being available at some point in the not too distant future. Any new design should use the OPA541 in the 11-pin TO-220 package.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hi Tim,
Figure 13 recommends fast recovery diodes but does not recommend a part number. Kindly recommend a fast recovery diode.
ES3BB-13-F
Additionally, it is recommended that transient voltage suppressor diodes be added from each supply pin to ground.
Also please confirm the filter capacitors chosen.
I presume you are speaking about the OPA541 power supply bypass capacitors? If so, 100 nF ceramic capacitors connected directly from the OPA541 V+ and V- pins to ground. Larger capacitance 10 uF capacitors are recommended on those power supply lines as well, but they can be located more distant from the V+ and V- pins.