This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yue,
THS4521 is Bandwidth: 145 MHz (AV = 1 V/V) Slew Rate: 490 V/µs and TLV9002 is Unity-gain bandwidth: 1 MHz. I see the simulation is 50Hz.
What is the purpose of the 760mV supply?
Here is a start. It still needs some tweaking.
Ron.
Thanks for the design , it's helpful. About the 760mv, I will check with them. basically, it is a bias.
So Yue,
I looked at that original THS4521 ckt - those are very high R values for a bipolar input FDA. If you need to use those, you might consider a CMOS FDA - kind of rare, but look at the
THS4520 or THS4521, 3.3V CMOS FDA's. The FDA provides a lot of advantages in how simple it is to set output CM voltage - I also notice a seperate op amp to drive the CM with Vcc/2. Most FDA's will default internally to Vcc/2 without an external driver - just needs a decoupling cap, not sure that is the case on the THS4520.
If you don't need to use those very high R's, move those down and look at the much improved (over the THS4521) THS4551 FDA.
Yue,
Here is circuit that needs only one TLV9002 and it shifts the output to center the -90mV input offset. If the 90 mV offset is useless information then I would suggest making the input AC coupled and making R1 and R6 200k ohms. Note V2 is not needed.