This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there,
I am looking for the most accurate current sense solutions for two situations:
1) 2 mOhm shunt where the voltage drop across can range from 7 mV to 25 mV
- CM Voltage range support from 2.8 to 4 V
- Bandwidth of at least 25 KHz
- A gain of at least 50 (the greater the better)
- Minimal gain error, offset voltage
Possible options I have found: INA190, INA191, INA240
2) 10 mOhm shunt where the voltage drop across can range from 11 mV to 24 mV
- CM Voltage range support from 5 to 14 V
- Bandwidth of at least 50 KHz
- A gain of at least 50 (the greater the better)
- Minimal gain error, offset voltage
Hello DanFer,
Best regards,
Ian Williams
Applications Manager
Current Sensing
Thanks for the feedback. What is the difference between the INA190 and INA191?
Are there any other options which are better fits but not mentioned by me?
Hi Dan,
The INA191 is the INA190 in a small wafer chipscale package (WCSP). The die is the same.
In terms of best offset voltage and gain error while meeting the required Vcm and bandwidth, these are the best fits.
Best regards,
Ian Williams
Thanks Ian. It looks like the INA190 and 191 have different accuracies. It looks like the 191 is more accurate with a lower offset voltage?
How can they be the same die? Is the difference in packaging causing these differences?
They are indeed the same die, but yes the package-level effects and the results of our characterization and test affect how we spec the datasheet. In truth the performance is extremely similar from one to the other - I doubt you would see much difference in the end application. Either way, they're both among the most precise current sense amplifiers in the industry, and offered for the same 1ku price.
Best regards,
Ian Williams
Just to back up what I'm saying with a quick calculation:
The minimum sense voltage in your first application is 7mV. The %error due to offset voltage is dominant at minimum input and is computed as simply (Vos/Vsense)*100.
Using typical offset:
Using maximum offset:
Best regards,
Ian Williams
DanFer, I will double-check the gain error vs. gain relationship for both parts and get back to you early next week.
Best regards,
Ian Williams
DanFer, I have confirmed with our test team that the datasheets are correct. They reflect some minor changes in our test system that were made for INA191, which came after INA190.
Best regards,
Ian Williams
That's right, or put another way, the A1 version at 25 V/V has just slightly worse gain error than the higher gain versions.
Best regards,
Ian Williams