This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
I want to measure two channels signal of 4-20mA and these two channels have to be isolated. How to use RCV420 do such function? Thanks,
Hi Charles,
If two channels have separate 4-20 mA sources and they are required to have their output voltages isolated from each other, that calls for two separate RCV420 devices. Attempting to use relays and other electronic components to provide complete isolation would could result in higher circuit complexity and cost compared to just using the two RCV420 devices.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hi Thomas,
Thank you for your response here. I just want to check for the two RCV420 solution, the power for these two amplifier need to be isolated? Right? Thanks.
Hi Charles,
Certainly, if complete galvanic isolation is required for each of the RCV420 channels.
Regards, Thomas
Precision Amplifiers Applications Engineering