This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a very small AC current, can RCV420 be used to get the proportional output.
If not which TI part can fulfil this requirement.
Thanks in advance.
Hi Dev,
Thank you for your question. How small is your AC current? What is your desired output? We may be able to do this with and Instrumentation Amp but I need know know the input / output requirements first.
-Tamara
Hi Dev,
I would guess that the RCV420 is optimized for currents between 4...20mA, or by other words currents in the milliampere range. If your current is much much smaller than this current range, then I would think that the RCV420 less suited for your application and that you should follow the recommendation given by Tamara.
Kai
Hi Tamara,
Following is my configuration:
Current is between 4mA to 20mA. and maximum voltage corresponding to this we want is 5V