Part Number: RCV420
Other Parts Discussed in Thread: TLV2333
Hi, I need 4-20mA input and output should be 0-3.3V. Is it possible with RCV420? Whether I need to use external circuits to bring it back from 5V to 3.3V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Joyson,
Yes, it is possible by connecting a resistor between CT (pin2) and +IN (pin 3), shorting IN- (pin1) and CT (pin 2), and using a voltage divider + opa buffer between REFOUT (pin11, pin10) and REFIN (pin12). I will look into this in detail and provide you an schematic. Please allow me 24 hrs.
Thank you and Regards,
Luis
HI Joyson,
Attached is a RCV420 configuration that will accept a 4mA-20mA input and produce approx. 0V-3.3V Output.
It requires a 143-Ohm resistor between CT (pin2) and +IN (pin 3), shorting IN- (pin1) and CT (pin 2), REFOUT and REFOUTFB shorted (pin 11, pin 10) connected to the voltage divider + OPA buffer to REFIN (pin 12) as shown on the schematic.
Thank you and Regards,
Luis
Dear Luis, thanks for the design. In our present design we do not have +12V & -12V supply. Is it be possible with +5V supply. We have 24V supply also.
HI Joyson,
The RCV420 requires bipolar supplies so it will not work without a negative supply.
You could easily build a discrete 4-20mA receiver using a dual amplifier and reference. The example below using the dual amplifier TLV2333 and REF3012 powers from a unipolar +5-V supply, accepts a 4-20mA input and produces a +100mV to +3.25V voltage output.
Thank you and Regards,
Luis