This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am looking for a VGA 10MHz , with -10 to +10 db gain operating with a single supply and single ended. Can VCA820 b e used with single power supply 10VDC? or can you suggest an alternative part number
Might be possible
1. All the signal path pins can operate with a single 10V supply as long as you observe their headroom limits to the supplies.
2. The output transimpedance amplifier has its non-inverting input pin brought out - bias that at mid supply with good noise decoupling - isolate that cap from the input transistors with a small 20ohm resistor to avoid emmitter follower self oscillation >1GHz.
3. The one unknown for me is that I believe the added ground pin is used as a reference for the Vg control input - the datasheet says that range is 0 to 2V assuming that ground pin I think. So, to run single 10V, put that ground pin at 5V and your gain control becomes a 5V to 7V range.
not 100% about this, but you might try it in TINA first.
Thanks Michael for you suggestion. I tried in TINA. VCA820 is functional only with dual supply .
Regards,
T Y JOSE
Hi Michael,
I have used a charge pump for negative supply and proceeded with my design.
Thanks
T Y JOSE