Hello HiRel team,
I'm looking for space-grade transimpedance amplifier. In terms of electrical parameters MAX3658A looks good, But I need radiation performance as well.
Best regards
Dmitry Tcholovsky
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello HiRel team,
I'm looking for space-grade transimpedance amplifier. In terms of electrical parameters MAX3658A looks good, But I need radiation performance as well.
Best regards
Dmitry Tcholovsky
Hello Michael,
I need to drive high speed photodiode, up to 1Gbps bitrate.
Best regards
Dmitry
Hey Dmitry,
We don't have a dedicated TIA in our space portfolio, you don't see very many of these in commercial either. You can configure a standard op amp, or in this case a fully differential amplifier as a transimpedance amplifier though. This blog post shows the basic connection: https://e2e.ti.com/blogs_/b/analogwire/archive/2013/10/25/how-to-build-a-tia-circuit-using-fully-differential-amplifiers
The best space part to use for this is going to be the LMH5401-SP.
Best,
Zak
Hello Zak,
Nice to see you.
Our meeting in Germany last January: as I remember you had some plans on TIA. Let me know of you need NDA.
LMH5401-SP looks overkill for my application.
Best regards
Dmitry Tcholovsky
Also, I did check out that 2013 e2e by Xavier - the THS4520 circuit looks wrong - that 1uF on the non-signal side is going to mess this - king of looks like it works,
Makes more sense that it is matched to the diode side, this is what the curve looks like in that e2e so I suspect the circuit was changed to this to run that plot,
And the LMH5401 might not be overkill
1. Source capacitance?
2. desired gain?
3. can you map your 1Gbit to a bandwidth requirement
Again is really sound like you are doing a optical digital comm requirement - the OCx amplifiers are transimpedance + comparator to diff out devices - digital output in essence.
Hello Michael,
Probably you are right about application :)
Capacitance: 1-3pF
Gain: my photodiode provides up to 5microA and I need ~250mV output signal.
With Maxim 580MHz Bandwidth I have about 650mbps.That is OK now. Looking for HiRel solution.
Best regards
Dmitry
Ok, that is a 50kohm gain assuming say 4pF max with FDA parasitic, the noise gain zero is at about 800kHz. To get 600Mhz closed loop Butterworth that will require a GBP of 4.5e14Mhz.
If I am doing this right, you might need two stages where something like the OPA855 front end at 1kohm transimpedance gain - but then that next gain of 50V/V with say 1GHz is not going to be one stage either.
So again, maybe this is really a much lower analog signal out of the transimpedance stage and then a comparator to take it to that differential 250mV digital output.
I'm open for different options. I'm looking for HiRel TIA and based on that chips around will be chosen.
Best regards
Dmitry
If you are constrained to space grade, just apps solutions won't get there - probably should be talking to the HiRel group in Dallas.
1. Do they have a fast single in to diff out comparator
2. Are there plans to make the OPA855 space grade?
But here is a starting point with the LMH5401 - using the commercial GBP, I can only get this much gain to provide around 600MHz GBP - I had to guess on the differential input C, 1pF, not specified and this sim suggests it is a little higher than that, this is only showing about 678ohm gain, so your 0 to 5uA will only be 3.3mV output.
here is what a +/-2.5uA at 100Mhz looks like
going to be tough noise wise, SNR to 1GHz is only 14dB
total output noise, which I think is RMS, is pretty high also -eventually would need like a 1GHz sharp filter to even get this good, if so, this would be 1.8mVpp noise 6X crest factor.
Hey Dmitry,
I apologize for the delayed reply, hope you are well. Yes we did discuss the possibility of releasing a high speed TIA for space comms, but we don't currently have any devices capable of meeting your requirement and do not have anything in the roadmap at this time. The fastest comparator we have for space is the LM119QML-SP, and this has a delay of ~30ns so it will be too slow for your application.
The best solution we have would be to use the LMH5401-SP in a TIA configuration and follow it with another LMH5401-SP to provide the gain you need. Though the bandwidth may seem overkill, when you factor in the parasitic capacitance and the gain you need as Michael has shown, it becomes very difficult to hit your target and is not possible in a single stage. Notice the Maxim part also integrates a second voltage gain stage after the TIA.
Again, the MAX3658 puts out a differential digital signal - that 2nd stage internally is more like a comparator. If you wanted to follow the LMH5401-S with a space grade comparator, look at the AD8561S