Other Parts Discussed in Thread: LM358, , INA293
Hello,
I am using INA199A1DCKR in one of my DC energy metering project for telecom applications.
DC voltage to be measured - 60VDC max using LM358 in differential mode
DC current to be measured - 100A max using 100A/50mV shunt from INA199
The 60VDC input to the system is fed to an isolated SMPS generating 5VDC for my control supply (for INA199 with ref pin connected to controller supply ground as well)
Same 60VDC is being monitored in differential mode
Current is being sensed in low side topology.
Since, the project is for telecom application; i am getting 48VDC GND as distribution terminal which is input to my DCEM shunt terminal; the other end of shunt is then fed to the load and positive terminal is directly connected to the load.
The issue is, as soon as i connect 48VDC GND (Isolated from 5VDC and GND which is supply to INA199) to shunt terminals (at this point load is not switched ON); INA199 is going to positive saturation and giving maximum output.
At this point, I am seeing -0.5VDC at both IN+ and IN- pin of INA199. I know its common mode range on lower side is -0.3V. May be this is causing INA199 to latch-up but it is not damaging.
I want to know what I can do to avoid this issue