This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH5401: High Frequency Single Ended Output

Part Number: LMH5401


Hello,

I am trying to use 6GHz of the LMH5401's 8GHz bandwidth. We would like to DC couple the output from a TI DAC that has an internal balun.

This would be a SE input, SE output application.

It seems that it is possible to use the LMH5401 as a SE output, but that might compromise the high frequency performance we will be needing. (from this blog)

Is the LMH5401 still our best device for this? Or is there a different amp you can recommend?

Thank you!

Regards,
Ryan B.