This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI C/C++ Compiler
Hello. I'm Seungmin.woo
I worked in enginner of isMedia.
These day, I'm developing new power board. so I want to use your opamp.
But, I meet the new difficult of problem.
In the tina
belows the picture, I want to make the 6V output.
Ideal Amp is OK, but OPA551 & TLV172 is incorrect.
Why?? T.T
Hello
Thank you for your appriciation.
I added to tina file.
please check this file: TOF.TSC
Hi Seungmin,
the TINA file didn't arrive. Please use the "Insert File" button (the paper-clip in the header).
Kai
Hi Seungmin,
you are violating the common mode input voltage range of OPAmp. See section 7.7 of datasheet of TLV172. You must stay 2V away from the positive supply rail.
Kai
Hello Kai,
Thank yor for your answer.
It is very helpful me.
Seungmin,
The model will not work that close to the positive rail. However the actual device will operate up to the positive rail at reduced performance and reduced test coverage.
See section 8.4.1 Common-Mode Voltage Range in the data sheet for this text and a table of typical performance. No limits specified and parameters may not be tested. So it is best to keep mode mode 2V below positive rail.
The input common-mode voltage range of the TLVx172 device extends 100 mV below the negative rail and within 2 V of the top rail for normal operation. This device can operate with full rail-to-rail input 100 mV beyond the top rail, but with reduced performance within 2 V of the top rail. Table 2 lists the typical performances in this range.
See data sheet for table 2.
within 2 V of the top rail for normal operation.This device can operate with full rail-to-rail input 100 mV beyond the top rail, but with reduced performance within2 V of the top rail. Table 2 lists the typical performances in this range.Table 2. Typical Performance for Common-Mode Voltages Within 2 V of the Positive SupplyPARAMETER MIN TYP MAX UNITInput common-mode voltage (V+) – 2 (V+) + 0.1 VOffset voltage 7 mVOffset voltage vs temperature 12 ìV/°CCommon-mode rejection 65 dBOpen-loop gain 60 dBGain-bandwidth product 0.3 MHzSlew rate 0.3 V/ìs
Hi Ron,
the phrase "reduced performance" in the datasheet sounds innocent. And the typical offset voltage of 7mV in table 2 of datasheet seems to be acceptable. But figure 3 shows a quite different picture:
One curve of 5 typical (!) units shows an offset voltage of nearly 50mV. And this is not even the end of the road...
Kai
Kai,
Well said. Offset can be quite high which is the main reason that the model aggressively discourages using the upper range. In some cases this could be acceptable. For a 36V unity gain signal, 50mV error at the top wouldn't be so bad. It's better than a phase reversal.
The TLV172 is phase reversal protected and not truly rail to rail input (compared to RRI parts that do a better job).