Part Number: LM7171
Hi team,
Are there any solution, especially the external compensation circuit for the input bias current of LM7171 in order to minimize DC error caused with the input bias current?
Best regards,
Iwata Etsuji
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM7171
Hi team,
Are there any solution, especially the external compensation circuit for the input bias current of LM7171 in order to minimize DC error caused with the input bias current?
Best regards,
Iwata Etsuji
Hello Iwata,
You can follow the method described in this article: https://e2e.ti.com/blogs_/archives/b/thesignal/archive/2012/04/11/input-bias-current-cancelation-resistors-do-you-really-need-them
This way both inputs will see the same resistance, and the voltages caused by the bias current will cancel each other. Note that both bias currents will not be exactly the same and you will still get some error because of this. You can look at the input offset current parameter to see the maximum difference between both bias currents.
Best,
Hasan Babiker
Yes, but this particular part has a high transconductance input stage where the the Ios is not much lower than the Ib (not matched that well).
Getting that high FPBW with good DC precision is a challenge, might publish an article on how to do that someday.
Michael-san,
Thank you so much for your comment!
I agree with you.
Hasan-san,
Thank you so much for your support.
I can understand what Bruce-san pointed out for the precision amplifiers.
While, I would like to double-check in the case of LM7171.
As you know, the each input of LM7171 is constructed with "diamond buffer" and each buffer drives the same load "RE".
In my understanding, the input bias current (especially its flowing direction) for diamond buffer is depending on its loading current, i.e. the direction of the each input bias current is opposite each other.
Therefore, the simple compensation circuit in the case of precision amplifier, such as "Rb", is not effective to LM7171, i.e. on the contrary to the case of the precision ampilier(with long-tail pair input circuit) there is no appropriate bias compensation circuit for LM7171 or some high speed amplifier with the similar input structure (Buffer + RE + CFB amp constructed with wilson-type current conveyor).
Is my understanding correct?
Best regards,
Iwata Etsuji
Hello Iwata,
Sorry for the delayed response. You are correct. Because of the structure of the LM7171, using the method of adding Rb to cancel the bias current is ineffective. However, we don't have an alternative method to minimize the bias current effects for this part.
Best,
Hasan Babiker