Hi,
I have some problems with using THS4531.
We knowTHS4531 is a differential op-amp that allows single-ended inputs
And the single-ended input voltages is 0-5V, how can I get the differential signals with 0-3V?
I have tried some methods, but it did not work.
I tried to reduce the 0-5V voltage to 0-3V input to the THS4531, and the output waveform is shown in the figure.
Looking forward to your help.