Hi,
We intend to use AFE031 for powerline communication.
When injecting a signal into power line using AFE031 and a coupling circuit, the output of the power amplifier reduces to 3Vpp from 6Vpp ( after LVCAP ). The transformer used is 1:1 ferrite cored having primary and secondary inductance of 300uH.
When tried to drive a inductive or resistive load directly from output of power amplifier, the amplifier is driving the current in order to maintain the voltage. But why is it not driving the current into power line?
regards