Part Number: XTR111
Hi,
i wish to use XTR111 for converting a +/- 10 V to +/- 20 mA. Please suggest if this device can be used for bipolar input as well.
Thanks
Venkatesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: XTR111
Hi,
i wish to use XTR111 for converting a +/- 10 V to +/- 20 mA. Please suggest if this device can be used for bipolar input as well.
Thanks
Venkatesh
Hi Venkatesh,
Kai is correct. The XTR111 is designed for the standard 0mA–20mA or 4mA–20mA analog signals, and can source up to 36mA.
-Tamara