This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear All,
I'm using the TL3472 to drive the excitation signal for a resolver. I would like to know if there are VOL and VOH vs IOUT values available for the TL3472 ?
Application conditions :
- power supply : +12V / 0V
- peak current : +/- 13 mA (sink and source)
The simulation with TINA TI shows about 1 V for VOL.
Can you give your feedback about this application ?
Thank you for your help.
Regards,
Christophe NINET
Hi Ninet,
I think the TL3472 in no good choice for your application because its guaranteed short circuit current is only -10mA and +20mA. See the bottom of page 4 of datasheet.
You should take an OPAmp with a stronger output stage.
May I ask, why did you take the TL3472?
Kai
Hi Kai,
Thank you for your feedback. This amplifier has been used in my company in a similar way but with less output current (the resolver input impedance was higher) and I hadn't noticed this output current limitations.
I'm considering using the ALM2402 instead (output current capability around 400 mA). I think this one is a better candidate ...
Have a nice day.
Christophe
Hello Cristophe,
Feel free to start a new thread if you need any help finding a new part.
Regards,
Daniel