This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV9002: Phase reversal

Part Number: TLV9002


It is stated on page 1 of the datasheet that there will be "no phase reversal" in overdrive conditions.

On page 16 it is stated that there is "no phase reversal" for an input voltage up to (V+)+0.1 V.

What I want to know though is if "no phase reversal" is guaranteed also in case you apply an input voltage more than (V+)+0.1 V but the input current through the op-amp internal diode from the input to the (V+)-rail is limited with resistors. A number of <10 mA is mentioned on page 13 in the datasheet under "Absolute maximum ratings". In my application the current would be limited to <1 mA