This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA128U Instrumentation amp output



Hi,
Can the output of the INA128U be shorted continuously without damage?

I am using instrumentation amp INA128U powered by +/-15 volts.
The INA128U provides a signal to a circuit that can only accept 8 volts maximum.
Can I place a 5 volt zener directly on the output of the INA128U to limit the voltage? 

In our circuit, during normal operation the output of the INA128U is in the range of +/-2 volts. But if our sensor input to the INA128U is wired incorrectly, the output of the INA128U can go to +15V.  So I need to protect the circut driven by the INA128U and make sure that the INA128U will not be damaged if I add a zener to limit the output voltage.
Thanks

  • Hello Lee,

     

    The absolute maximum rating for output current is continuous, but I would still recommend trying to limit that current by placing a resistor on the output.  You may want to add a pad during your layout.  Please note that the output will also be limited by the forward voltage of the diode, which may make your -2V output challenging.