Part Number: INA180
Other Parts Discussed in Thread: LM324, TINA-TI, INA181
Bidirectional output current from INA180?
In my design, I would like to offset the output of an INA180 with a resistive summing function. For this to work correctly, the INA180 output would need to sink current (such as 1 mA or less) under some conditions. An op amp such as LM324 can source or sink output current, but I see no mention of output current sinking capability in the INA180 datasheet. Of course no amplifier is perfect. I know that any output current variation will cause a small gain or offset error. But let's say that changing the output load current (positive out of the amplifier) from -500 uA to -1 mA should not introduce much more error than changing the output load current from +500 uA to + 1 mA.
If the INA180 is not capable of sinking current without introducing significant error, I can design around this with an added op amp buffer or other means. Can you please let me know?