Part Number: LOG114
Other Parts Discussed in Thread: OPA2196, OPA196, LMC6081, LMP7721
I want to measure both positive and negative current using the same log114 amplifier. Is it possible?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Kai,
I have seen this section. But in my application the current can also be positive in some cases. So instead of using the above circuit i need a circuit where I can measure current of both polarities i.e., negative and positive.
Hi Ravi,
it depends on your application. Can you tell more about your project?
Kai
Hi Ravi,
The TI LOG amplifiers including LOG114 are unidirectional input current devices. That is dictated by the unidirectional current flow through he logging transistors used in the feedback of the input op amp transimpedance stages. See Figure 1 in the datasheet for details about the input stages.
Maybe if we learn more about your application we can offer some ideas.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hi thomas and kai,
Our application is to use the log 114 as an ammeter. It should be able to show the absolute value of current irrespective of the direction of current i.e, we should be able to measure both negative and positive current(+7mA to -7mA). As pointed out by Kai we need to change the polarity of current and we should make it positive only(make it unidirectional as pointed out by thomas). Please give me suggestions for the same because the current is very small.
Hi kai,
My current source is a known voltage source in series with an unknown resistance which is to be measured.
Dear Kai,
No it does not generate AC but the user can apply voltage from any direction.
Ravi
Hi Ravi,
can you show a scheme? What measuring voltage are we talking about? What range of resistance is to be measured? Why is the maximum current limited to +7mA of -7mA? Is this a short current limting? Provided by a resistor?
Kai
Hi Ravi,
I am not sure where you found that particular LOG114 model in TINA? When I check TINA for the LOG114 "Spice Macro" this much more detailed symbol is provided:
I am not sure what the A and B inputs correspond to, I1 and I2? And then what is IREF?
You are certainly aware that the LOG114 cannot be powered with a 700 V supply so that is something must have been overlooked in your simple schematic. Also, be aware that if the intended input voltage is 700 V that is a very high voltage level. The PC board environment and the potential for severe over voltage of low voltage ICs is a real possibility. Working with high voltage required much precaution compared to working with low voltage.
I realize that you want to maximize the current measurement resolution, but the LOG114 doesn't really appear to be the solution. Have you considered a conventional op amp transimpedance amplifier (TIA) operated from dual polarity supplies? It won't provide the resolution of a LOG amplifier, but it will readily accommodate the bipolar input current. The high voltage concerns would apply to it as well.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hi thomas,
I am not powering the log 114 with 700v power supply. Here is the schematic as per above model. In this schematic the resistance R2 has to be calculated which maybe upto 1.5 teraohms(current in picoamperes) so we cannot measure it using conventional op amp transimpedance amplifier. The current through the log114 is controlled by the source itself so it will not exceed 10mA.
Hi Ravi,
The first scheme 1 you show is connected as the LOG114 is intended, but scheme 2 is not. I recall if you attempt to operate the LOG114 in this manner the logging transistor has no current flow through it, the transimpedance gain becomes enormous and VLOGOUT rails. And note that even when the input current is flowing in the correct direction the minimum specified input current is 100 pA so it is not usable in picoampere applications having current levels lower than the 100 pA minimum.
I have looked for ways to accommodate a bipolar LOG114 input current, but every idea has resulted in one or more issues that make them unacceptable.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hi Thomas,
Is there any possibility to use circuit such as precision rectifier to change the polarity of current in scheme 2?
Regards, Ravi
Hi Ravi,
I had considered applying an absolute value circuit before the LOG114 input, but it looks like much of the resolution will be lost. The absolute value circuits are voltage input circuits. It would require the wide range +/- input current be converted to a voltage range for the absolute value circuit to act upon it.
The problem is the absolute value circuit, and even the LOG114 operating in voltage input mode (See Voltage Input on Pg. 18 of the LOG114 datasheet) can't match the 7 to 8 decades of dynamic range the LOG114 provides in current input mode. The datasheet states, "Voltage inputs may be handled directly by using a low-impedance voltage source with series resistors, but the dynamic input range is limited to approximately three decades of input voltage." Therefore, the high resolution needed to detect the very low currents would not be attainable.
Here is a link to a Burr-Brown Applications Bulletin (AB121) that describes precision absolute value circuits.
http://www.ti.com/lit/an/sboa068/sboa068.pdf
If you have any ideas after looking it over please share them.
Regards, Thomas
Precision Amplifiers Applications Engineering
Kai,
Thanks for providing a practical implementation of a switchable TIA and absolute value amplifier circuit. I agree with your selection of the LMC6081 for the TIA and the OPA196 (or OPA2196 dual) for the absolute value amplifier circuit.
You are certainly aware of the construction and PC board cleanliness requirements needed to obtain precision TIA performance when used at very low input current levels. Ravi may not be as familiar with the practical TIA implementation requirements.
Your application circuit would be usable down to tens or hundreds of picoamperes on its highest TIA gain range with proper construction and cleanliness. The LMP7721, which is femptoampere input current op amp, has a very good Application Note that goes into the details required to maintain the very low input current performance of such op amps.The Application Note information could prove useful for a practical LMC6081 TIA circuit. It is provided here for reference:
http://www.ti.com/lit/ug/snou004/snou004.pdf
Regards, Thomas
Precision Amplifiers Applications Engineering