Dear Sir,
I am using an INA199A1DCK (sampled) in a standard shunt monitoring application.
Vvcc = 12V, Vref = 5V, Bidirectional. Rshunt = 50mOhm. The circuit is protected with a R/C filter and a dual zener diode (AZ23C24), as shown in the datasheet.
The Vcm is within the specified range.
The resistors used for the filter (two resistors both in series with IN+ and IN-) are 2k2. Concluding from the datasheet this would give a gain of 45.
It does not though, the gain becomes 17. I verified the marking of the INA199A1 to be correct.
I removed the zener diode and capacitor to eliminate influence, and so there is only the shunt, two 2k2 resistors and then the INA199A1 inputs.
Still the gain stays 17.
Any idea how this can happen?