Part Number: LMC6062
Other Parts Discussed in Thread: OPA277, LM4040, LMC6061
Hi
I asked a question to my orignial request
I've done the current generator seen on previous article based on a LMc6062 and reference voltage
The current generator with the 91Khoms is about 27 uA
The INA 114 on the schematic is not assembled and a OPA277 in following mode is connected to the load resistor to measure the value
I've set up 5 generator on a card and I meet a strange problem
The 5 are totaly identical but
When I applie the power sometimes 2 of the 5 generator are not starting and deliver 0 UA
By puting power supply on / OFF / ON several times the 2 failing generators becomes OK
the load of the generator is between 100 K and 300 Kohms .. but the value seems not to disturb
Have you any idea .?
thanks in advance
Regards