Part Number: INA188
Other Parts Discussed in Thread: LM7705
Hi
is it possible to use IN188 to make an active 4-20mA inout ?
And to only power supply it in 0V-24V .
See diagramm below :
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Cyril,
your information is a bit confusing. Is it 4...20mA or +/-20mA or 0...20mA?
You will need to connect a negative supply voltage to the V- pin of INA188. Depending on your input signal current, a LM7705 might eventually be sufficient.
Kai
Hi,
it is for 0....20mA & 0---10V only.
but as VCM spécification is (VS-)+0.1V. I think i need a offset. isn't it ?
Thanks