Why the input at positive and negative, the result are different
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The 180 degree phase difference is because one is non-inverting the other inverting.
The gain difference is that for non-inverting, Cf can only lower gain towards 1V/V; while for inverting Cf can reduce gain towards 0V/V.
Remember that noninverting gain is 1+RF/R1 while inverting gain is -RF/R1
The gain difference is that for non-inverting, Cf can only lower gain towards 1V/V; while for inverting Cf can reduce gain towards 0V/V.
I still confused
why non-inverting,Cf can only lower gain towards 1V/V and inverting Cf can reduce gain towards 0V/V this part could you explain in detail please
The explanation for that statement is that at high frequencies the capacitor can be considered a short. In the case of non-inverting configuration, if the capacitor is a short the op amp is in a buffer configuration, which has a gain of 1V/V. If the capacitor is a short in the inverting configuration, it bypasses the opamp in the signal path, thus giving a gain of 0V/V.
Mathematically where CF shorts out RF
Non Inverting gain is 1+RF/R1 so gain is 1 + 0/1k = 1
Inverting gain is -RF/R1 so gain is -0/1k = 0
I understand what's your mean, for non-inverting configuration at the high frequency the gain will be 20log(1V/V) =0dB ,
but for inverting configuration 20log(0V/V) is wrong value and the gain is -20dB ?
With a perfect op amp the forward gain curve will continuously falls with frequency. The gain of a real op amp drops with higher frequency so it can not produce an ideal response.
Your mean is 20log(0V/V) is falling?
but at high frequency there is a zero and pole right? I still don't understand this part
I agree you said real op amp drop with higher frequency but how to explain 20log(0V/V)