Hi,
Good day. I hope you are doing fine.
Our customer is using the LM7321 and they have inquiry about the minimum voltage at IN+ pin. Kindly refer to the inquiry below.
"I know for a power source there is a minimum 2.5+ VDC, but for the signal that it is amplifying which I believe is IN+ on the pin configuration from the datasheet, is there a minimum voltage that should be here? Right now I have .03 VDC here with a gain of 11, but it seems to be only giving me an output voltage of .203 which is around a 6.7 gain"
I hope you could help us with this matter. Thank you for your kind support.
Regards,
Cedrick