Part Number: THS4505
Other Parts Discussed in Thread: THS4504, THS4551, THS4561,
In accordance with the data sheet the common-mode input range of THS4504/4505 at Vs=5V (single supply) is from -0.1 to 2V over temperature (see page 7 of the data sheet). In the second side there is an example of a fully differential line driver with high output swing (see figure 81 of the data sheet) where the common mode is 7.5V at Vs=15V. My circuit is a transformer driver based on the fully differential configuration with input common-mode voltage is 2.5V (see attached file). If this OK?